How can we help you today?

Is the QOM2 breaker available with a field-installable or factory-installed shunt trip?

Product Line:
Circuit Breakers

Resolution:
The QOM2-VH breakers are available with shunt trip factory installed only.
The shunt trip is rated 120, 208, or 240 Vac. For the shunt trip, add the suffix 1021 to the circuit breaker catalog number.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings