Issue:
What are the acceptable wire sizes and torque values for the GV1G09 and GV2G05?
Product Line:
Digest 177 Section 16 : Nema and Definite Purpose and Starters
Environment:
North American Products
Resolution:
Solid cable:
(1) #14 to #2 AWG conductor or
(2) #14 to #6 AWG conductors
Flexible cable without cabel end:
(1) #14 to #2 AWG conductor or
(2) #12 to #6 AWG conductors
Flexible cable with cabel end:
(1) #14 to #4 AWG conductor or
(2) #14 to #10 AWG conductors
Tightening Torque:
Connector = 20 lb-in
Screw Clamp = 15 lb-in
What are the acceptable wire sizes and torque values for the GV1G09 and GV2G05?
Product Line:
Digest 177 Section 16 : Nema and Definite Purpose and Starters
Environment:
North American Products
Resolution:
Solid cable:
(1) #14 to #2 AWG conductor or
(2) #14 to #6 AWG conductors
Flexible cable without cabel end:
(1) #14 to #2 AWG conductor or
(2) #12 to #6 AWG conductors
Flexible cable with cabel end:
(1) #14 to #4 AWG conductor or
(2) #14 to #10 AWG conductors
Tightening Torque:
Connector = 20 lb-in
Screw Clamp = 15 lb-in
Released for: Schneider Electric Canada