In a 3 phase, QO load center, is a backfed main breaker with the PK3MB retaining kit restricted to a certain position?
Issue:
Where can the PK3MB retaining kit be mounted in a 3 phase, QO load center?
Product Line:
QO 3-phase Main Lug Load Centers
Resolution:
Yes. It is only intended for use in the upper left side of the interior. This will be in breaker spaces 1, 3 and 5. There is NOT a retaining kit for mounting a 3 phase, backfed main breaker on the upper right side of the panel or in any other location.
Where can the PK3MB retaining kit be mounted in a 3 phase, QO load center?
Product Line:
QO 3-phase Main Lug Load Centers
Resolution:
Yes. It is only intended for use in the upper left side of the interior. This will be in breaker spaces 1, 3 and 5. There is NOT a retaining kit for mounting a 3 phase, backfed main breaker on the upper right side of the panel or in any other location.
Released for: Schneider Electric Canada


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.