Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will A type thermal units or B type thermal units work in lieu of AR type thermal units?
Issue:
Can A and B Type of thermal units be used instead of AR Heaters?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
9065 Type S Overload relays

Resolution:
No, these are not interchangeable. The AR thermal units are for use in a bimetallic overload relay where the A & B types are melting alloy style.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings