Product Line:
NEMA style Overload Relays
Resolution:
The standard Motor Logic does not have an option for automatic reset. However, through the use of remote reset module and a timing relay the automatic reset function can be accomplished. See attached link for additional information on this option.
The Motor Logic Plus does provide automatic reset function as standard.
NEMA style Overload Relays
Resolution:
The standard Motor Logic does not have an option for automatic reset. However, through the use of remote reset module and a timing relay the automatic reset function can be accomplished. See attached link for additional information on this option.
The Motor Logic Plus does provide automatic reset function as standard.
Released for: Schneider Electric Canada