Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can XB5 / ZB5 operators be used in XACA pendant stations?
Issue:
Are the XB5 / ZB5 operators compatible with XACA style pendant stations, where the XEN-G style contact blocks are installed ?

Product:
Push Buttons and Pendant Stations

Environment:
XAC, XEN , XB5, ZB5

Answer:
No. There are no pendants stations that are approved to use with the XB4 / XB5 operators at this time.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings