Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the clear lens for the 2510 devices with pilot lights?
Issue:
Looking for a part number for the clear lens for the 2510 devices with pilot lights?

Product Line:
NEMA and Definite Purpose Contactor and Starter

Environment:
North American Products

Resolution:
The lense is included with the replacement 9999PL pilot light kits or can be obtained separate by ordering part number 31057-037-03.

This applies to Class 2511 & Class 2512 units which also use the 2510 Type F & K base devices.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings