How can we help you today?

What is the rating of the number of switching operations of Square D, 200 A, general duty, F-series safety switches?

Product Line:
GD SS

Resolution:
For safety switches, the standard for design and testing of the number of switching operations is governed by UL98 and NEMA KS-1. There are two separate tests: (1) Endurance Test, and (2) Horsepower-overload test. The below table shows the minimum number of operations required (OFF to ON to OFF) by UL and NEMA. For the endurance test, however, Square D F series safety switches exceed the UL and NEMA requirements by up to 3 times the total (see below table):

NUMBER OF OPERATIONS
Square D Safety Switches (F series)
200 A, General Duty

Endurance Test Number of OpsHP Test Number of Ops
Test StandardAt Rated Load*No LoadTotal (L+NL)At Rated HP
UL60002000800010
NEMA 60002000800010
Square D6000180002400010

*Endurance test done at switch rated load current
**Horsepower test - make/break motor inrush/locked rotor current at rated HP