Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement contact module for the class 9002 type AW13,14,15, and 133 foot switches?
Issue:
Looking for the replacement module for a 9002AW13,14,15,and 133.

Product Line:
Push Buttons and Operator Interface

Environment:
9002A Foot Switches

Resolution:
9007CO3 is the replacement contact module for the 9002 AW 13,14,15, and 133.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings