Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the operating handle of a KA225AWK circuit breaker enclosure be padlocked in the ON position?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Cause:
Application

Resolution:
The provisions to padlock the operating handle in the ON position are not a standard enclosure feature. For field modification, a 3/8`` maximum hole can be drilled in the Lockoff Slider to allow the handle to be locked in the ON position. Check local code regulations for acceptability. Paint metal areas exposed by drilling with PK49SP touch-up paint.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings