Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What parts are required to add start stop push buttons on a NEMA 1 enclosed Class 8911 Definite Purpose starter?
Issue:
Looking for the parts required to field add start stop push buttons on a NEMA 1 enclosed Class 8911 Definite Purpose starter.

Product Line:
8911 Definite Purpose Starters

Environment:
NEMA Contactors and Starters

Cause:
Field installing start stop push buttons.

Resolution:
The parts required depends on the starter size; select the proper components based on the following:

For 20 through 40 amp devices (DSG & DPSG) devices; DPB1.
For 50 amp devices; 9999BLX and 9999SA2.
For 60 through 90 amp devices: side mount Class 9001 Type K units.

Note: Holding circuit contacts are not provided with 8911 definite purpose starters. For 8911DPS units use 9999D10 auxiliary, for 8911DS compact units auxiliary contacts are not available and other means of holding circuit must be supplied or maintained control contacts must be used.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings