Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for replacement 110 / 120 vac control coil for the LC1F400 contactor?
Issue:
LC1F400 replacement coil for 110/120Vac

Product Line:
IEC Contactors and Starters

Environment:
Tesys F Contactors

Resolution:
For standard coil (40 - 400 hertz) order LX1FJ110.

For low sealed consumption coil (40 - 400 hertz) which offers high tolerance to inrush voltage drops, immune to micro-breaks (main supply or contact chain) and are capable of operation on networks with harmonic numbers less than or equal to 7; order LX9FJ925.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings