Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the 9001 type K and SK rated for NEMA 3R?
Issue:
NEMA ratings for the 9001 type K and SK push buttons

Product Line:
Push Buttons and Operator Interface

Environment:
9001 Type K and SK Push Buttons

Resolution:
Yes, they are rated NEMA 1, 2, 3, 3R, 4, 6, 12, and 13. The 9001 SK devices are also rated NEMA 4 X.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings