How can we help you today?

Control Expert on Windows 10, receiving error message when trying to build project on running process.

Issue

Occasionally returns "the thread tried to read from or write to a virtual address for which it does not have the appropriate access" error.

Product Line

Control Expert, Unity Pro

Resolution

Sometimes this error can be a conflict with something else that is installed on the PC. It might require a repair or reinstall in the end.
(For repair, launch setup.exe from the DVD files)

Before a repair/reinstall you can try launching from a shortcut with properties set as below as sometimes this will correct it.

From the Shortcut tab select Run As Administrator.

134528_IMG

From the Security Tab set all permissions to allow for all users/groups. Special permissions do not matter.

134528_IMG1

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings