Is there a way to display Frequency value in Percentage on ATV320 and ATV340?
Issue:
How do I setup the ATV320 or ATV340 HMI to display percentage 0-100% instead of 0-60hz?
Product Line:
ATV320 ATV340
Resolution:
Follow procedure attached ( it's for ATV340 but it is same for ATV320).
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
Released for: Schneider Electric Canada