How many 175 A or 200 A branch circuit breakers may be installed in a NQ Panelboard?
Issue:
Is it possible to install 175A or 200A branch breakers in an NQ Panelboard?
Product Line:
NQ Panelboard
Environment:
Application
Resolution:
Up to four (4) 2 pole QO2175, QO2200, QO2175VH, or QO2200VH circuit breakers may be installed in 400 A and 600A NQ single phase panelboards in NEMA 1 enclosures, with three-point latch trim fronts. NQ200AN neutral lug kits are required if neutral connections are required for any of these branch circuit breakers.
Is it possible to install 175A or 200A branch breakers in an NQ Panelboard?
Product Line:
NQ Panelboard
Environment:
Application
Resolution:
Up to four (4) 2 pole QO2175, QO2200, QO2175VH, or QO2200VH circuit breakers may be installed in 400 A and 600A NQ single phase panelboards in NEMA 1 enclosures, with three-point latch trim fronts. NQ200AN neutral lug kits are required if neutral connections are required for any of these branch circuit breakers.
Released for: Schneider Electric Canada