How can we help you today?

Can explosive atmosphere XB4 be ordered as components?

Issue:
Can GEX explosive atmosphere operators be separately purchased?

Product line:
Pushbuttons, Switches, Pilot Lights, Control Stations and Joysticks

Environment
Harmony XB4 signal units for explosive environments

Cause:
Long lead time, looking for options

Resolution:
Only the complete refrences as XB4***GEX are fitted with the specific gasket needed to have the certification, no sub-assemblies are available, that means not ZB4***GEX products are availables.

This gasket isn't sold as a spare part.

The contact block ZBVBM1GEX is available only for spare parts.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: