What are the GS2 Disconnects DC ratings?
Issue:
What is the maximum DC current and voltage for the GS2 Disconnect switches?
Product line:
Operating Mechanisms and Disconnect Switches
Environment:
TeSys GS2
Cause:
Customer requires to use it up to 600Vdc
Resolution:
Switches are rated up to 250Vdc, see attached table extracted from 9421CT0301R03/16 Page 28
What is the maximum DC current and voltage for the GS2 Disconnect switches?
Product line:
Operating Mechanisms and Disconnect Switches
Environment:
TeSys GS2
Cause:
Customer requires to use it up to 600Vdc
Resolution:
Switches are rated up to 250Vdc, see attached table extracted from 9421CT0301R03/16 Page 28
Released for: Schneider Electric Canada