How can we help you today?

How can you read outlet pressure high alarm on the ATV630 drives over serial communications?

Resolution:

ST08 address is 16108 and bit 5 will give you high alarm status.

Bit 0: (DRYA) : Dry Running Alarm

Bit 1: (PLFA) : Pump Low Flow Alarm

Bit 2: (HFPA) : High Flow Alarm

Bit 3: (IPPA) : Inlet Pressure Protection Alarm

Bit 4: (OPLA) : Outlet Pressure Low Alarm

*Bit 5: (OPHA) : Outlet Pressure High Alarm

Bit 6: (PCPA) : Cyclic Start Protection Alarm

Bit 7: (JAMA) : Antijam alarm is raised

Bit 8: (LFA) : Low Flow Alarm

Bit 9: (LPA) : Low pressure alarm is raised

Bit 10: (FSA) : Flow limit function activated (FL_Mode_On)

Bit 11: (OPSA) : Outlet Pressure High Switch Alarm

Bit 12: (MPCA) : Multi-pumps Capacity Alarm

Bit 13: (MPLA) : Multi-pumps Lead Alarm

Bit 14: (LCHA) : Level Control High Level Alarm

Bit 15: (LCLA) : Level Control Low Level Alarm

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us atdrive.products.support@se.comto create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Canada
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
  • Product Selectors