Does HCR24NALCU comes with a CT?
Issue:
Wants to know if the HCR24NALCU comes with a CT
Product Line:
I-Line
Environment:
Neutral kits
Cause:
Product information
Resolution:
No. It does not have any Neutral Current Transformer. You can decipher if the Additional lugs have a Neutral Current Transformer if the part number have a "CT" suffix. Here is an example, page 3 : https://download.schneider-electric.com/files?p_enDocType=Data+Bulletin&p_File_Name=2110PD9501.pdf&p_Doc_Ref=2110PD9501
Released for: Schneider Electric Canada