Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Schneider Electric / Square D offer NEMA Type 7 or 9 Circuit Breaker Enclosures for use in hazardous environments?

Issue:
Product Design Features

Product Line:
Circuit Breaker Enclosures

Cause:
Selection

Resolution:
CBE = Circuit Breaker Enclosures
SCCR = Short Circuit Current Rating

Square D does offer a few CBE Types rated for NEMA 7 or 9, hazardous locations. See the current ON-LINE Digest for the catalog numbers.

The NEMA 7 and 9,  CBE use Molded Case Circuit Breakers and are available For the PowerPact B-Frame breaker from 15 to 30Amps, 2 and 3 pole breakers. Also, available for the PowerPact
J-Frame breaker from 150-225Amps 2 and 3 pole. These devices are cULus Listed, unless otherwise noted in the current digest. The SCCR of the device is equal to the rating of the circuit breaker installed unless otherwise noted in the digest.