How can we help you today?

Can 50A breaker be used to protect the HEPD80?

It is not recommended to use a 50A circuit breaker to connect the HEPD80 to the panel electrical bussing due to the HEPD80 uses wire size #12 and the circuit breaker should be sized accordingly. The HEPD80 is UL1449 TYPE 1 and does not even require to be connected to any over current protection device but we do recommend to connect the HEPD80 to a dedicated 20A 2P CB if possible.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: