How can we help you today?

How is ethercat address set on the ATV320 drive?

Address value ECAA is a read only value. The address must be assigned via the PLC controller.

Please make sure to power cycle the device once the address has been forced through the controller.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions: ​

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team. ​

If you are not located in North America, please contact your local Customer Care Center for assistance: ​

Schneider Electric Canada
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
  • Product Selectors