Energy meter kit with Bacnet communications
Issue
Looking to purchase an Energy Meter Kit with Bacnet communications.
Resolution
The default configuration of the Energy Meter kit comes with the iEM3455 which only supports modbus communications. The model number iEM3465 supports Bacnet communications. If Bacnet is required, the components would need to be purchased separately as in the example below.
| Part Number | Description |
| A9MEM3465 | iEM3465 energy meter - BACnet - 1 DI - 1 DO - multi-tariff - LVCT |
| EM3500ENC | PowerLogic EM3500 - Mounting option enclosure with door - for 1 EM35xx series |
| EMFP1, EMFP2, or EMFP3 | Fuse packs - Select correct fuse pack for number of phases being monitored EMFP1 - 1 phase EMFP2 - 2 phase EMFP3 - 3 phase |
| LVCT's | See Table below for LVCT part numbers |
Released for: Schneider Electric Canada
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.