In the old MPZ transformers, can you swap the old primary circuit breaker from FAL to a Powerpact H-frame?
Product Line:
Mini-Powerzone, Low Voltage Transformer
Environment:
Mini-Powerzone, Low Voltage Transformer
Cause:
Need to know if the factory supplied primary FAL circuit breaker in an MPZ15S40F transformer can be replaced by a Powerpact H-frame in the field.
Resolution:
The FAL and HDL breakers have different dimensions/sizes and use different sheet metal, so the H-frames can not be swapped on the field. Customer will have to replace the entire unit with the new style MPU15S40F.
Released for: Schneider Electric Canada