How can we help you today?

What is the ratio of the 9070 Industrial Control Transformers

Issue: Industrial Control Transformers Ratio

Product Line: Industrial Control Transformers

Answer: The 9070 Industrial Control Transformers are purposely built with what is known as Compensation. This means that they will deliver the full rated voltage output voltage even when fully loaded to their maximum allowable Secondary amperage. This also means that the Secondary voltage when the unit is unloaded will skew quite high. Compensation does reduce the winding ratio which will differ from the mathematically derived voltage ratio of simple 2:1 or 4:1. 240:120 or 480:120.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings