How can we help you today?

Locating 8901DPA* Coil Voltage

Issue:
Locating part number on 8910 Definite Purpose Contactors

Product Line:
Contactors

Environment:
Definite Purpose Contactors

Resolution:
Coil voltage can be found on the top portion of the 8910DPA** contactor.
*Refer on below photo*

Example voltage codes:
24Vac = V14
120Vac = V02
208-240Vac = V09
480Vac = V04
600Vac = V07

Sample part number: 8910DPA12V02 (120V)


8910DPA Coil Voltage