Does NQ panelboard come standard with bonding strap?
Issue:
NQ panelboard not quoted as service entrance rated.
Product line:
NQ panelboard
Resolution:
For Factory Assembled NQ panelboard:
- Yes IF the factory assembled panel is selected to be service entrance rated and;
- No IF the factory assembled panel is not selected to be service entrance rated.
- For bonding strap part numbers see FA125473 .
For RTI NQ panelboard:
- Yes all RTI NQ panelboard part numbers on the digest catalog comes with bonding strap as standard.
Released for: Schneider Electric Canada