Replacement Motor for KZG/KZH Series Erie Actuator
Issue:
Need a replacement motor for an existing KZ series Erie Actuator
Product Line:
Erie Actuator, Erie Zone Valves, KZ Series Two-Position PopTop Zone Valves
These are Kele Zone Valve and Actuator manufactured by Erie
Resolution:
The replacement motor depends on the voltage rating of the actuator, see part number below:
- 30-158-A KZG/KZH Series actuator replacement motor, 24 VAC
- 30-158-B KZG/KZH Series actuator replacement motor, 110/120 VAC
- 30-158-D KZG/KZH Series actuator replacement motor, 208 VAC
- 30-158-T KZG/KZH Series actuator replacement motor, 277 VAC
- 30-158-U KZG/KZH Series actuator replacement motor, 230/240 VAC
Released for: Schneider Electric Canada