Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How much force does it take to operate the QOM1-VH main circuit breakers?

Issue:
Product Design Features

Product Line:
QO and Homeline load centers

Resolution:

From OFF to ON, it takes 9 lbs of force.

From ON to OFF, it takes 4 lbs of force.

From TRIP to OFF, it takes 11 lbs of force.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings