How can we help you today?

Is an SD Card required to operate a Tesys Island TPRBCEIP?

Issue:
Need to know if the SD card is required

Product Line:
Motor Management system Tesys Island

Environment:
IEC Contactors and Starters

Resolution:
TeSys island bus couplers are designed with a card slot for a micro SD card. The island maintains files on the micro SD card for the fast device replacement (FDR) function, as well as a software/firmware backup from the device and log files.

The SD card is not mandatory and is only there for backup purposes

NOTE: If used, It is recommended to backup the SD card data regularly.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings