How can we help you today?

How do I use/wire the Digital IO module TPRDG4X2?

Issue:
Is voltage provided from the island for the inputs and outputs of TPRDG4X2?

Product Line:
Motor Management system Tesys Island

Environment:
IEC Contactors and Starters

Resolution:
The digital inputs require an externally supplied 24V signal to drive them high. Simply shorting I0 to IC will not drive the input high.

The digital outputs will connect and disconnect an externally supplied 24V source. The 24V is not derived from the island itself, it must be supplied by the user.
TPRDG4X2 wiring

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings