Can I use a mix of single phase and three phase in Tesys Island Avatars?
Issue:
Need to know if it is possible to mix single-phase and 3-phase loads in Tesys Island.
Product Line:
Motor Management system Tesys Island
Environment:
IEC Contactors and Starters
Resolution:
Yes, you can use a mixture of single phase and three phase Avatars in your system. If doing this, you must configure the "island" (VIM) as three-phase, and wire it A-B-C. Then for any single-phase avatars, they must be wired with phase A in the line 1 connection and phase C in the line 3 connection. The single-phase voltage must be Line-Line. At the moment TeSys island does not support energy monitoring for single-phase voltages L-N if the entire system is three-phase.
Need to know if it is possible to mix single-phase and 3-phase loads in Tesys Island.
Product Line:
Motor Management system Tesys Island
Environment:
IEC Contactors and Starters
Resolution:
Yes, you can use a mixture of single phase and three phase Avatars in your system. If doing this, you must configure the "island" (VIM) as three-phase, and wire it A-B-C. Then for any single-phase avatars, they must be wired with phase A in the line 1 connection and phase C in the line 3 connection. The single-phase voltage must be Line-Line. At the moment TeSys island does not support energy monitoring for single-phase voltages L-N if the entire system is three-phase.
Released for: Schneider Electric Canada
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and en expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.