How can we help you today?

For Tesys Island, what is the accuracy of Current Measurement?

Issue:
Unable to find current accuracy for Tesys Island systems

Product Line:
Motor Management system Tesys Island

Environment:
IEC Contactors and Starters

Resolution:
Per our technical literature and marketing specs, all we publish is an energy monitoring accuracy which is 10% for loads running under nominal conditions(50–125%FLA, power factor 0.7, 47–63Hz).

The current measurement is accurate enough to satisfy all protection functions per UL/IEC 60947-4-1 and to satisfy this 10% energy monitoring requirement. This represents various accuracies at various levels of current relative to FLA. Not published: Under nominal environmental conditions, at 50 or 60hz, and running near FLA, the current measurement is 2% accurate.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings