undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
​​​​​​​Tesys Island mounting and ambient temperature deratings
Issue:
Can the Tesys Island be mounted vertically without derating?

Product Line:
Motor Management system Tesys Island

Environment:
IEC Contactors and Starters

Resolution:
TeSys island standard starters, SIL2 starters, and power interface modules are designed for operation without derating under the following conditions:
• Horizontal mounting position
• Ambient temperature up to 50 °C (122 °F)

For vertical mounting or ambient temperatures above 50 °C (122 °F), apply the derating values in the following table to the load rating requirements. If both derating conditions apply, then you must apply both derating factors. Derating is calculated by the digital tools.

derating Tisland

The derating conditions apply to all standard starters, SIL starters, and power interface modules. The derating conditions do not affect short-circuit protection devices.

Schneider Electric Canada

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: