What is a minor event in Tesys Island and how to fix it?
Issue:
Examples of minor events and how to fix them for Tesys Island
Product Line:
Motor Management system Tesys Island
Environment:
IEC Contactors and Starters
Resolution:
When the island encounters a minor event, the fieldbus and service ports remain activated. The only avatar activated is the System avatar.
All starters, SIL starters, and I/O modules are de-energized, defined as follows:
• Starters and SIL starters are in the open state
• Outputs from the I/O modules are off (set to zero)
See the attached extracted page from the user guide with corrective actions.
Released for: Schneider Electric Canada