Are the 80034-187-02 and the HLW1BL the same?
Issue:
How to order 80034-187-02?
Product Line:
Panelboards
Resolution:
Yes, the 80034-187-02 and the HLW1BL are the same. The 80034-187-02 is an interplant item that was offered before if the customer needs only 1 pc of HLW1BL. The HLW1BL is a kit that contains Qty 3 of 80034-187-02.
Released for: Schneider Electric Canada