Will the HCM91TSD work in place of HCM91TSVD?
Issues:
Can the HCM91TSD trim be used instead of HCM91TSVD?
Product Line:
I-line Panelboard
Resolution:
Yes it can be used in place of the HCM91TSVD. However, if the application needs the vented, will have to use the HCM91TSVD or it might have heat rise issues that will void the warranty.
Released for: Schneider Electric Canada