How can we help you today?

What is the maximum branch circuit breaker that can be installed in an HCN I-Line panel?

Issue:

Largest breaker that can be installed in an HCN I-line panel

Product Line:

I-Line Panelboards

Resolution:

The largest breaker that an HCN panelboard can accept is a max of 225A for the Q frames and max of 150A for the H frame. J frames will not fit.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings