Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you put a 200A branch breaker on a NQSE142400S?

Issue:
Need a 200A branch breaker for NQSE142400S

Product Line:
Panelboards.

Environment:
Products sold in Canada

Resolution:
Replacing the NC62VS cover with an NC62VS3P and adding an NQ200AN neutral lug would allow you to add the QO2200 or QO2200VH breaker. The reason for the 3-point latch trim is that the 200A branch breaker requires it so that the door remains shut in the event of a short circuit.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings