How can we help you today?

Tesys Island Update firmware message in SoMove

Issue:
Getting a Tesys Island Update firmware message in SoMove
Tesys Island Firmware update message

Product Line:
Motor Management system Tesys Island

Environment:
IEC Contactors and Starters

Resolution:
The DTM you have used to connect to the TeSys Island is detecting an older version of firmware that is incompatible. Update your TeSys island firmware to the compatible version, then proceed.
To update the firmware, you can save the DTM project (or open a new instance of SoMove) and connect to the device (do not store a configuration, load one) and do firmware update.  Then go back to your configuration and store it.

Refer to the attached Release Notes to find a compatibility matrix between the Tesys Island Firmware and DTM versions.

Schneider Electric Canada

Attachment(s)
TeSys Island Firmware 3.2 Release notes DOCA0224EN-2 - 6_2023.pdf [1.63 MB]
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings