What is the maximum branch circuit breaker that can be installed in an HCJ I-Line panel?
Issue:
Verify the maximum branch circuit breaker that can be installed in an HCM I-Line panelboard.
Product Line:
I-Line Panelboards sold and supported in the USA.
Environment:
Application
Cause:
Product selection.
Resolution:
250 amp J frame I-Line breaker is the maximum that will mount in an HCJ panel.
Released for: Schneider Electric Canada