Does the NF panelboard interior comes comes with the phase barriers? What is the part number?
Product Line:
NF Panelboard
Environment:
NF Panelboard Interior
Cause:
Need to verify if the NF442L2 panelboard comes with the phase barriers (black plastic phase barrier between the lugs inside an NF panel) and how many it comes with.
Resolution:
Yes, the NF panel interior comes with phase barriers (black plastic insulator/barrier between main lugs on NF panel). The part number is 80113-550-01. It comes with Qty 4 of 80113-550-01.
Released for: Schneider Electric Canada