Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Tesys Island Error Message: before configuring the Tesys Island update the firmware
Issue:
Somove does not allow to configure the Tesys Island due to a firmware issue, see message:

Tesys Island firmware update needed
Product Line:
IEC Contactors and Starters

Environment:
Tesys Island Motor Management System

Resolution:
The DTM you have used to connect to TeSys island is detecting an older version of firmware that it knows is incompatible.  Check the release notes and ensure you are using the right DTM, updated your TeSys island firmware to the compatible version, then proceed.

Note in order to update firmware, you can save the DTM project (or open a new instance of SoMove) and connect to the device (do not store a config, load one) and do firmware update.  Then go back to your configuration and store it.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings