How can we help you today?

8538 and 8539 NEMA Combination Starters OSHPD Label

Issue:

Need to know if 8538 and 8539 Combination Starters come with OSHPD Label

Product Line:

8538 and 8539 NEMA Combination Starters

Environment:

NEMA Contactors and Starters

Resolution:

By default, OSHPD Label is not included on the Combination Starter Enclosure. They can be factory modified by adding the form "G31" under the Enclosure options.

There is no field installable option for this one, only factory installed option.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: