How can we help you today?

Protection for EMI (Electromagnetic interference) on NSYCRN54200

Issue:

Do we offer NSY enclosures that have EMI / EMC (Electromagnetic interference / disturbances)?

Product Line:

Universal Enclosures

Environment:

NSY S3DC & S3HF Enclosure series

Resolution:

No, the NSYCRN54200 does not have EMI Protection

There are two option for enclosures that will have EMI or EMC protection.

NSYS3DC series - Page 58-77 standard against electromagnetic disturbances (treated with Aluzinc)

NSYS3HF series - Page 338-340 The enclosure surface, comprising 55 % aluminium ensures good reflection of radiated electromagnetic interference. (Page 340)

See Link: https://download.schneider-electric.com/files?p_Doc_Ref=9993CT0901&p_enDocType=Catalog&p_File_Name=9993CT0901R08_16+Body+(Web).pdf

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: