Is the 7400FMB floor mounting bracket compatible with EXN transformers?
Issue:
Need to know if the 7400FMB floor mounting bracket compatible with EXN45T3H transformer.
Product Line:
General Purpose Dry Type 600 Volts and Below Transformer
Environment:
EXN transformers
Resolution:
The 7400FMB is an external part to the enclosure and will fit all EXN series Transformers, but is seldom needed since the EXN enclosures already have mounting holes located in the bottom of the enclosure frame.
Released for: Schneider Electric Canada