Is the I-Line panelboard IP2X rated?
Product Line:
I-Line Panelboard
Environment:
Low Voltage Panelboard
Cause:
Need to verify if I-Line panels are IP2X rated.
Resolution:
No, IP2X is only available on NQ panelboard. I-line does not have IP2X offerings. I-Line panelboards have custom barrier offerings which can be selected through the product selectors and provides load side breaker lug shields and a barrier over the Neutral assembly. However, this does not have an official finger safe rating either.
Released for: Schneider Electric Canada