What is the MCOV rating for Model# 425480DP10AWAJ10?
Product Line:
ASCO Surge Device
Environment:
Surge Protection Device
Cause:
Need to confirm if the MCOV of Model# 425480DP10AWAJ10 is rated 115% above nominal voltage.
Resolution:
As per VPR chart on Page 2 shows an MCOV of 552V which is exactly 115% above nominal voltage. That is 480V x 1.15 = 552V.
Released for: Schneider Electric Canada