What is the replacement for EE112T1814HFISNLP?
Issue:
Replacement for part number EE112T1814HFISNLP.
Product Line:
Low voltage Transformers
Answer:
This is something that would be built in SE Advantage/product selector. Please see the break down of the catalog:
EE-112-T-1814-HF-IS-NLP
EE is our transformer product line, Energy Efficient. This is replaced by our EX/EXNs.
112 - is for 112.5kVA
T - 3-phase
1814 - 480V Primary to 480Y/277V Secondary
HF - for 115 deg C Temp Rise
IS - Isolation Shield
NLP - Non-linear, K13 listed (this would be selected on the first part where it says EX/EXNs)